STM8AF52AATCY CAN_Configuration in halt mode
Dear Sir/Madam,
Now I did controller into halt completely. But when it's in halt mode if any GPIO external interrupt is triggered means it wakes up, but when I will send the CAN Identifier then It's not waking up. As per data sheet in halt mode if CAN_RX interrupt comes it should wake up. So, can you please guide to me what initialization I need configure for CAN before entering into the halt mode. Here I added CAN_Config(); function.
void CAN_Config(void)
{CAN_InitStatus_TypeDef status = CAN_InitStatus_Failed;/* Filter Parameters */
CAN_FilterNumber_TypeDef CAN_FilterNumber;FunctionalState CAN_FilterActivation;CAN_FilterMode_TypeDef CAN_FilterMode;CAN_FilterScale_TypeDef CAN_FilterScale;uint8_t CAN_FilterID1;uint8_t CAN_FilterID2;uint8_t CAN_FilterID3;uint8_t CAN_FilterID4;uint8_t CAN_FilterIDMask1;uint8_t CAN_FilterIDMask2;uint8_t CAN_FilterIDMask3;uint8_t CAN_FilterIDMask4;/* Init Parameters*/
CAN_MasterCtrl_TypeDef CAN_MasterCtrl;CAN_Mode_TypeDef CAN_Mode;CAN_SynJumpWidth_TypeDef CAN_SynJumpWidth;CAN_BitSeg1_TypeDef CAN_BitSeg1;CAN_BitSeg2_TypeDef CAN_BitSeg2;uint8_t CAN_Prescaler;/* CAN register init */
CAN_DeInit();/* CAN init */
CAN_MasterCtrl=CAN_MasterCtrl_AllEnabled;//CAN Loop Back Mode JNa//CAN_Mode = CAN_Mode_LoopBack;CAN_Mode = CAN_Mode_Normal;/*CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;
CAN_BitSeg1 = CAN_BitSeg1_5TimeQuantum;CAN_BitSeg2 = CAN_BitSeg2_2TimeQuantum;CAN_Prescaler = 4;*/CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;
CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum;CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum;CAN_Prescaler = 8; /* 500kbit/s */status = CAN_Init(CAN_MasterCtrl, CAN_Mode, CAN_SynJumpWidth, CAN_BitSeg1, \
CAN_BitSeg2, CAN_Prescaler);/* CAN filter init */CAN_FilterNumber = CAN_FilterNumber_0;CAN_FilterActivation = ENABLE;CAN_FilterMode = CAN_FilterMode_IdMask;CAN_FilterScale = CAN_FilterScale_32Bit;CAN_FilterID1=0; CAN_FilterID2=0;CAN_FilterID3=0;CAN_FilterID4=0;CAN_FilterIDMask1=0;CAN_FilterIDMask2=0;CAN_FilterIDMask3=0;CAN_FilterIDMask4=0; CAN_FilterInit(CAN_FilterNumber, CAN_FilterActivation, CAN_FilterMode, CAN_FilterScale,CAN_FilterID1, CAN_FilterID2, CAN_FilterID3,CAN_FilterID4,CAN_FilterIDMask1, CAN_FilterIDMask2, CAN_FilterIDMask3, CAN_FilterIDMask4);/* Enable Fifo message pending interrupt*/
/* Message reception is done by CAN_RX ISR*/CAN_ITConfig(CAN_IT_FMP, ENABLE);}Here, I am suspecting about my configuration, what configuration need to be change.