cancel
Showing results for 
Search instead for 
Did you mean: 

vs platform io _can msgs in loopback mode not happening

optimus_pRime
Associate

i was trying to work on bluepill stm32f103c6t6 i triedto send can msgs in loopback mode but im not able to see the mssg in cro for the pins pa11,12 (tx,rx) can somebody help me out . the folowing code i have used for that 

#include "stm32f1xx_hal.h"
#include <stdio.h>

// CAN message structure
CAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[5] = {0xAA, 0xBB, 0xCC, 0xDD, 0xEE}; // Sample data
uint32_t TxMailbox;

// Add global variable to store CAN handle
CAN_HandleTypeDef hcan;

// UART handle and buffer
UART_HandleTypeDef huart1;
char uart_buffer[100];

// Function prototypes
void CAN_Configuration(void);
void UART_Init(void);

void CAN_Configuration(void) {
    // Initialize CAN peripheral and other settings
    // ...

    // Configure the CAN settings (CAN ID and speed)
    hcan.Instance = CAN1;
    hcan.Init.Prescaler = 4; // Set the prescaler to achieve 500 Kbps (assuming 8 MHz APB1 clock)
    hcan.Init.Mode = CAN_MODE_LOOPBACK; // Enable Loopback Mode
    hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
    hcan.Init.TimeSeg1 = CAN_BS1_8TQ;
    hcan.Init.TimeSeg2 = CAN_BS2_3TQ;
    hcan.Init.TimeTriggeredMode = DISABLE;
    hcan.Init.AutoBusOff = DISABLE;
    hcan.Init.AutoWakeUp = DISABLE;
    hcan.Init.AutoRetransmission = ENABLE;
    hcan.Init.ReceiveFifoLocked = DISABLE;
    hcan.Init.TransmitFifoPriority = DISABLE;

    // Start the CAN peripheral
    if (HAL_CAN_Init(&hcan) != HAL_OK) {
        // Error handling (optional)
        while (1);
    }
}

void UART_Init(void) {
    huart1.Instance = USART1;
    huart1.Init.BaudRate = 115200;
    huart1.Init.WordLength = UART_WORDLENGTH_8B;
    huart1.Init.StopBits = UART_STOPBITS_1;
    huart1.Init.Parity = UART_PARITY_NONE;
    huart1.Init.Mode = UART_MODE_TX_RX;
    huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
    huart1.Init.OverSampling = UART_OVERSAMPLING_16;

    if (HAL_UART_Init(&huart1) != HAL_OK) {
        // Error handling for UART initialization failure
        while (1);
    }
}

int _write(int file, char *ptr, int len) {
    HAL_UART_Transmit(&huart1, (uint8_t*)ptr, len, HAL_MAX_DELAY);
    return len;
}

int main(void) {
    // Initialize HAL, GPIOs, and other peripherals
    // ...

    // Initialize UART for debugging
    UART_Init();

    // Initialize the CAN peripheral in Loopback Mode
    CAN_Configuration();

    // Configure the CAN message header
    TxHeader.StdId = 0x400;    // Set the CAN ID to 0x400
    TxHeader.ExtId = 0;        // Not used in standard CAN mode
    TxHeader.RTR = CAN_RTR_DATA; // Data frame (not a remote frame)
    TxHeader.IDE = CAN_ID_STD;   // Standard ID format (not extended)
    TxHeader.DLC = 5;          // Data Length Code (number of bytes in TxData)
    TxHeader.TransmitGlobalTime = DISABLE; // Optional: DISABLE or ENABLE

    while (1) {
        // Send the CAN message
        if (HAL_CAN_AddTxMessage(&hcan, &TxHeader, TxData, &TxMailbox) != HAL_OK) {
            // Error handling for transmission failure
            printf("Transmission failed!\r\n");
        } else {
            printf("CAN message sent successfully!\r\n");
        }
       
        // Wait before sending the next message
        HAL_Delay(1000); // 1 second delay between messages
    }
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0