cancel
Showing results for 
Search instead for 
Did you mean: 

StdPeriph_Driver for STM8AF6223

Posted on May 10, 2017 at 18:25

I use the IAR embedded workbench IDE (version 2.20.2)

I have to change  the project from STM8S003 to STM8AF6223.

in the project options i have set the correct device and added the file stm8s_tim5.c and deleted the file stm8s_tim2.c

in the actual used library STM8S_StdPeriph_Driver I have uncommented the line

&sharpdefine STM8AF626x */    /*!< STM8A Medium density devices */

to switch from STM8S003 to the medium density devices (STM8AF622x/4x)

compiling the project returns a lot of errors related to TIM5.

where can I get the actual release of the needed driver library for the STM8AF6223 ?

thanks for your response!

#stdperiph_driver #iar-embedded-workbench #stm8af6223
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0