cancel
Showing results for 
Search instead for 
Did you mean: 

Some questions about ADC in SMT8S.

VPatr.2
Associate II

Hi, everyone. I have been working with STM8S, i am did not work with this microcontroller before, i have some questions about ADC (i am using STM8S103F3).

1) The first problem that i had was about the values read, i am initialize the peripheral for work with multiple channel using scan mode. So, the value is read one time, after i need deinitialize and initialize the adc peripheral in the while main for get a new value. I was reading the manual and i found about "Buffer overrun flag" , how can i resolve that problem? I am using stm standard library. 

2) The second is about the channels that i need read. Below is my code, i get one channel value, but i dont get multiple values because all adc buffer has the same value. I need change the register during the program for change the channel?

main() {

SystemClockConfig();

TIM4_Setup();

GPIO_Setup();

UART1_Setup();

ADC1_Setup();

while(1){ 

if(millis() - timeoutLed > 1000){ 

ADC1_ScanModeCmd(ENABLE);

ADC1_StartConversion();

while(ADC1_GetFlagStatus(ADC1_FLAG_EOC) == FALSE);

ADC1_ClearFlag(ADC1_FLAG_EOC);

a2Value = ADC1_GetBufferValue(2);

a3Value = ADC1_GetBufferValue(3);

vH = a2Value >> 8;

vL = a2Value & 0xFF;

UART1_SendData8(vL);

UART1_ClearFlag(UART1_FLAG_TXE);

delay(5);

UART1_SendData8(vH);

UART1_ClearFlag(UART1_FLAG_TXE);

delay(5);

vH = a3Value >> 8;

vL = a3Value & 0xFF;

UART1_SendData8(vL);

UART1_ClearFlag(UART1_FLAG_TXE);

delay(5);

UART1_SendData8(vH);

UART1_ClearFlag(UART1_FLAG_TXE);

delay(5);

ADC1_Setup();

timeoutLed = millis();

GPIO_WriteReverse(GPIOB, GPIO_PIN_5);

}

}

}

void ADC1_Setup(void){

ADC1_DeInit();

ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS,

ADC1_CHANNEL_2,

ADC1_PRESSEL_FCPU_D18,

ADC1_EXTTRIG_GPIO,

DISABLE,

ADC1_ALIGN_RIGHT,

ADC1_SCHMITTTRIG_CHANNEL2,

DISABLE);

ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS,

ADC1_CHANNEL_3,

ADC1_PRESSEL_FCPU_D18,

ADC1_EXTTRIG_GPIO,

DISABLE,

ADC1_ALIGN_RIGHT,

ADC1_SCHMITTTRIG_CHANNEL3,

DISABLE);

ADC1_ConversionConfig(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_2 | ADC1_CHANNEL_3 , ADC1_ALIGN_RIGHT);

ADC1_DataBufferCmd(ENABLE);

ADC1_Cmd(ENABLE);

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0