Same functions ; different result
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-12-17 7:15 AM
Posted on December 17, 2013 at 16:15
I am using STM8L-Discovery board, STVD and Cosmic Compiler 32k; and ST peripheral libraries(stn8l15x.h file revision number is 1.4/2010)
I have runned the next code:#include ''stm8l15x.h''#include ''delay.h''void main(void) {//initializare pini GPIO_DeInit(GPIOA); GPIO_DeInit(GPIOE); // GPIO_Mode_In_FL_No_IT = (uint8_t)0x00, /*!< Input floating, no external interrupt */ //GPIO_Mode_In_PU_No_IT = (uint8_t)0x40, /*!< Input pull-up, no external interrupt */ // GPIO_Mode_In_FL_IT = (uint8_t)0x20, /*!< Input floating, external interrupt */ //GPIO_Mode_In_PU_IT = (uint8_t)0x60, /*!< Input pull-up, external interrupt */ //GPIO_Mode_Out_OD_Low_Fast = (uint8_t)0xA0, /*!< Output open-drain, low level, 10MHz */ //GPIO_Mode_Out_PP_Low_Fast = (uint8_t)0xE0, /*!< Output push-pull, low level, 10MHz */ //GPIO_Mode_Out_OD_Low_Slow = (uint8_t)0x80, /*!< Output open-drain, low level, 2MHz */ //GPIO_Mode_Out_PP_Low_Slow = (uint8_t)0xC0, /*!< Output push-pull, low level, 2MHz */ //GPIO_Mode_Out_OD_HiZ_Fast = (uint8_t)0xB0, /*!< Output open-drain, high-impedance level, 10MHz */ //GPIO_Mode_Out_PP_High_Fast = (uint8_t)0xF0, /*!< Output push-pull, high level, 10MHz */ //GPIO_Mode_Out_OD_HiZ_Slow = (uint8_t)0x90, /*!< Output open-drain, high-impedance level, 2MHz */ //GPIO_Mode_Out_PP_High_Slow = (uint8_t)0xD0 //PA6- input - button; PE4- output-led GPIO_Init(GPIOA,GPIO_Pin_6,GPIO_Mode_In_PU_No_IT ); GPIO_Init(GPIOE,GPIO_Pin_4,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_0,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_1,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_2,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_3,GPIO_Mode_In_FL_No_IT ); GPIO_Init(GPIOE,GPIO_Pin_5,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_6,GPIO_Mode_Out_OD_Low_Slow); GPIO_Init(GPIOE,GPIO_Pin_7,GPIO_Mode_Out_OD_Low_Slow); GPIO_WriteBit(GPIOE,GPIO_Pin_All,RESET); //pin PE3 is resetting as well; but it does not through error while(1){ if(GPIO_ReadInputDataBit(GPIOA,GPIO_Pin_6)) { delay_ms(100); GPIO_ResetBits(GPIOE,4); delay_ms(100); GPIO_SetBits(GPIOE,(uint8_t)4); } else { delay_ms(40); GPIO_WriteBit(GPIOE,GPIO_Pin_4,RESET); delay_ms(40); GPIO_WriteBit(GPIOE,GPIO_Pin_4,SET); }} }I have runned the programm; the led stays off permanently; if I push the button( equivalent with putting to GND the PA6 pin); the led starts blinking.I have looked at those functions definitions from library; they are the sane; or if is a hidden stuf in there, it should do the same thing.void GPIO_WriteBit(GPIO_TypeDef* GPIOx, GPIO_Pin_TypeDef GPIO_Pin, BitAction GPIO_BitVal){ /* Check the parameters */ assert_param(IS_GPIO_PIN(GPIO_Pin)); assert_param(IS_STATE_VALUE(GPIO_BitVal)); if (GPIO_BitVal != RESET) { GPIOx->ODR |= GPIO_Pin; } else { GPIOx->ODR &= (uint8_t)(~GPIO_Pin); }}/** * @brief Writes high level to the specified GPIO pins. * @note The port must be configured in output mode. * @param GPIOx : Select the GPIO peripheral number (x = A to I). * @param GPIO_Pin : Specifies the pins to be turned high. * @retval None */void GPIO_SetBits(GPIO_TypeDef* GPIOx, uint8_t GPIO_Pin){ GPIOx->ODR |= GPIO_Pin;}/** * @brief Writes low level to the specified GPIO pins. * @param GPIOx : Select the GPIO peripheral number (x = A to I). * @param GPIO_Pin : Specifies the pins to be turned low * @retval None * @par Required preconditions: * The port must be configured in output mode. */void GPIO_ResetBits(GPIO_TypeDef* GPIOx, uint8_t GPIO_Pin){ GPIOx->ODR &= (uint8_t)(~GPIO_Pin);}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0