2018-09-19 4:24 AM
We are interfacing "DS1307" RTC chip with STM8L152C6 Discovery board using I2C polling method.
with clock setting as mentioned bellowed .
void clock_setup(void)
{
static uint32_t Clock_frequency = 0;
CLK_DeInit();/*Deinitializes the CLK peripheral registers to their default reset values.*/
CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);/*Configures the System clock (SYSCLK) source System Clock Source HSI.*/
CLK_HSICmd(ENABLE);/*Enables Internal High Speed oscillator (HSI)*/
CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_2);/*Configures the System clock (SYSCLK) dividers.System Clock Divider: 16 */
CLK_PeripheralClockConfig(CLK_Peripheral_I2C1,ENABLE);/*Peripheral Clock Enable 2, ADC1*/
Clock_frequency = CLK_GetClockFreq();/*Returns the frequency of the System clock (SYSCLK)*/
}
void GPIO_setup(void)
{
GPIO_DeInit(GPIOC);
GPIO_Init(GPIOC, GPIO_Pin_0,GPIO_Mode_Out_OD_HiZ_Fast); /*SDA pin as PC0*/
GPIO_Init(GPIOC, GPIO_Pin_1,GPIO_Mode_Out_OD_HiZ_Fast); /*SCL pin as PC1*/
}
After this setting
void I2C_setup(void)
{
I2C_DeInit(I2C1);
I2C_Init(I2C1,I2C_MAX_STANDARD_FREQ,0xD0,I2C_Mode_I2C,I2C_DutyCycle_2,I2C_Ack_Enable,I2C_AcknowledgedAddress_7bit);
I2C_Cmd(I2C1,ENABLE);
}
flag2 = I2Cx->SR3; /*This flag always remain at 0x02 hence I2C communication is not getting started */
Always BUSY flag in set (1) Hence I2C communication is not completed. function name.
ErrorStatus I2C_CheckEvent(I2C_TypeDef* I2Cx, I2C_Event_TypeDef I2C_Event)
flag2 = I2Cx->SR3; /*This flag always remain at 0x02 hence I2C communication is not getting started */