cancel
Showing results for 
Search instead for 
Did you mean: 

LINKER error during compilation. Basically we are migrating from STM8AF6246TASSSX to STM8AF6266TCX which is basically the same family. We created a new project and include the source files. But finding issue in Linking.

BSidd.1
Associate II

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Ok, might be helpful to be specific about the actual error message.

E​dit the question so the title/summary and the body of the question are separate, and add salient detail and context.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

1) can't locate checksum segment

2) segment .ubsct size overflow (85)

3) no default placement for segment .RUN_TIME_BUF

4) no default placement for segment .CLASS_B

5) no default placement for segment .STACK_BOTTOM

6) no default placement for segment .CLASS_B_REV

If needed lets have a teams call to discuss it . Let me know your contact please.