In stm8s0003f3 ,I am reading analog voltage.I am getting the value in watch as 1544,which is not expected .Can some one help what may be the fault in the code. supply vge is 1.8v
void Init_ADC(void)
{
ADC1_DeInit();
ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D2,
ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,DISABLE);
}
void ADC_Read(unsigned int MV)
{
ADC1_DeInit();
ADC1_Init(ADC1_CONVERSIONMODE_CONTINUOUS, ADC1_CHANNEL_5, ADC1_PRESSEL_FCPU_D2,
ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_CHANNEL5,DISABLE);
ADC1_StartConversion();
MV=ADC1_GetConversionValue();
ADC1_Cmd(ENABLE);
while(ADC1_GetFlagStatus(ADC1_FLAG_EOC) == FALSE);
ADC1_ClearFlag(ADC1_FLAG_EOC);
ADC1_Cmd(DISABLE);
}