cancel
Showing results for 
Search instead for 
Did you mean: 

I2c pcf8574-Ds1307--

debruyne.marc
Associate II
Posted on February 20, 2013 at 20:58

hello,

after long trying, i managed to write to the pcf8574

in assembly language.

no i have only a problem with WRITING to the DS1307, i can read the DS1307

my question is, when you use a crystal of 14.7456Mhz, what are the correct settings in the freq ,and ccrl registers, because i have connect the DS1307 to the AARDVARK and i can write and read.

are there special precautions for write to a DS1307

many thanks

marc debruyne

#duplicate-thread
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on February 21, 2013 at 14:17

You already have a thread open on this topic:

/e08bd40b

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.