cancel
Showing results for 
Search instead for 
Did you mean: 

Debug/programming another chip with STLINK from STM8disco

thibaut2
Associate II
Posted on August 30, 2012 at 12:11

Hi,

After developping and testing with stm8s-discovery connected to various evalboards, i just received my prototype.

As written in STM8SVLDISCOVERY's usermanual, i unsoldered the two 0 Ohms of swim connector from the STLINK (i don't want to break the discovery board yet).

Now, i disconnected everything on my board (thru jumpers), except external power-supply to the micro, and i connected SWIM port and GND.

The Chip i use is the STM8S105S4, and i already changed the device target.

Using STVD/Cosmic, i try to enter debug mode and i receive this message :

 

Starting debug session...

 

 -> Emulator reset (usb://usb)...

 

  ** Connection error (usb://usb): swim error [30006]: comm init error: chip does not answer

 

 

 -> Failed to connect target.

Seeing SWIM_reset pin, i also connected it (althrough SWIM = SingleWire) and i get same message :\

What did i miss ?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
thibaut2
Associate II
Posted on August 30, 2012 at 14:26

Well... I went for lunch, and after the break, everythin worked fine....

I guess the computer was hungry too ^^