STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Starting Stm8s GPS speed device

Posted on May 15, 2011 at 19:19Hello, At the beginning, I must say that I am a beginner in microcontrolers... I have to project GPS speedometer device based on stm8s discovery, LCD(nokia 3310), GPS module and some kayboard, I have all the parts, but...

pietruha8 by Associate II
  • 1118 Views
  • 3 replies
  • 0 kudos

UART2 Interrupt

Posted on June 24, 2010 at 10:36Hello i'm port uart2 polling receive data from hyperterminal it's ok. but i need use uart2 receive data with interrupt?   TIM3_DeInit();     TIM3_TimeBaseInit(TIM3_PRESCALER_1,0xFFFF);    TIM3_ITConfig(TIM3_IT_UPDATE...

uthenb by Associate II
  • 829 Views
  • 3 replies
  • 0 kudos

UART Problem - Garbage characters in UART Example/Demo

Posted on April 24, 2011 at 23:47Hi.Today I started playing with the STM8-DISCOVERY board, and I tried the RS232/UART example from your website: http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/um0884.zipAfter having installed...

tkjmail2 by Associate II
  • 1653 Views
  • 3 replies
  • 0 kudos

STM8L1526 EVAL ST-LINK USB DRIVER

Posted on May 06, 2011 at 10:10Where can I find USB driver for STM8L1526 Evaluation board on Windows XP machine to connect as ST-Link.

pradeep by Associate
  • 483 Views
  • 0 replies
  • 0 kudos

From AVR (AVR-GCC) to STM8 with STM8S-Discovery

Posted on May 05, 2011 at 16:31Good day! I'm writing my first project with STM8. Here are a couple of questions: - AVR-GCC has a convenient attribute PROGMEM (http://www.nongnu.org/avr-libc/user-manual/pgmspace.html) to store data (for example big a...

artvolk by Associate II
  • 671 Views
  • 0 replies
  • 0 kudos

SPI Slave Mode Clock Settings

Posted on April 29, 2011 at 14:46Hi, is it required to setup the prescaler in SPI slave mode? And why can i scope a clock of 1Mhz, if i set a prescaler of 2 (f_Master/2) in master mode whereas i have an oscillator of 16Mhz. (standard STM8S-Discovery...

tnn1985 by Associate II
  • 1226 Views
  • 1 replies
  • 0 kudos

Slave select (NSS) pin management of SPI

Posted on April 26, 2011 at 15:10Hi all, Is there anyone who can give me some advice about the STM8S SPI? I tried to setup STM8S105 as the SPI master mode with the hardware slave select management mode which is transmit only mode. Here my source cod...

0690X00000603OUQAY.jpg

Firmware Library

Posted on April 11, 2011 at 17:08Where can I get the Discovery firmware library? The page stm8sfwlib no longer exists. Graybeard

radiation from mobile phones -> auto reset?

Posted on April 19, 2011 at 10:42Hello, I have just finished my project, but unfortunately I have a problem at the end. ;) My Stm8s Discovery is in a plastic box together with a cell phone. When the cell phone get switched on, the microcontroller re...

master by Associate II
  • 640 Views
  • 1 replies
  • 0 kudos