cancel
Showing results for 
Search instead for 
Did you mean: 

Any pointers on how code for the STM8S should be written...

Posted on April 29, 2010 at 15:12

Hi there,

I've noticed that the structure for the files architecture has changed dramatically from what I was used to...

So I could do with some help getting started...

It appears things have moved on from having header files and long chunks of code and it now appears that the norm is to break the code down into it's various function blocks and keep each function as a seperate source file...

While I try and resolve the current issue I have of getting the code to compile, can I at least start to look at the STM8 code that has already been submitted or will these also need to be tweaked for the STM8S Discovery...

Only the main function I initially require once I have the RS232 talking is to start talking to the I2C and having it store hourly data...

So any help on this would also be greatfully received...
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0