cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32CubeProgrammer with active UART over ST-LINK/V2

Yood
Associate II

While working with NUCLEO-H743ZI​ board I noticed that if my already burned program use the UART port over the USB (multiplexed with ST-LINK/V2) I can't earse the FLASH using the STM32CubeProgrammer.

Earsing the image with IAR IDE and program the FLASH with program that don't use the UART solve the problem and now I can erase the image with STM32Cube Programmer.

Is it a known problem that the STM32CubeProgrammer is not working with an active UART port over shared ST-LINK/V2 USB ??

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0