cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProg v.2.17.0 wrong BOR Level on STM32U0xx

Pypke
Associate

Hi,

Controller STM32U073, programming with STM32CubeProg v2.17.0 ist the BOR Level in option byte wrong.

Programing the option byte with the framework,  for example generated code with CubeMX works.

 

Bug Report

 

2 REPLIES 2
TDK
Super User

This could really be presented better. In what way is it wrong? What steps are you taking and what results are you seeing that are different from what you expect?

If you feel a post has answered your question, please click "Accept as Solution".
STTwo-32
ST Employee

Hello @Pypke 

If you are reporting about the fact that the BOR bits on the STM32U0 MCU series is set to 6 on the Factory settings, this issue has been raised to the Dev team for correction (under internal ticket number 189186):

STTwo32_0-1724331648403.png

Best Regards

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.