2023-07-17 12:05 AM - edited 2023-07-17 12:06 AM
While installing the program for my windows 10 it hangs at step 8 which is shortcuts set ups. So I have been reaserching the internet and forums for a while still didn't manage to find a solution
2023-07-27 3:15 AM - edited 2023-07-27 3:20 AM
I have the same problem and still can't find a solution. I tried the setup in 4 computers and only one of them was successful and it was a coding pc which had many applications installed so maybe there is a software package that needs to be installed.
2023-07-27 4:35 AM
2023-07-27 9:11 AM
Hello,
Yes, I tried using admin rights, different folder, 32-64 bit installers, installing java versions etc.
Best Regards.
2024-05-15 3:00 AM
We have the same problem. Tried on many computers. No luck. Anybody solved this problem on Windows 11?
2024-06-17 1:12 AM - edited 2024-06-17 1:12 AM
I believe this problem is related to your Windows Language. I had the similar issue in the past and changed my Windows language to English. Everything worked fine after that.
2024-12-10 7:46 AM
I was having this problem too. Your solution works. The language pack should be English for windows. Thanks.
2026-02-13 11:08 AM
Even though I've set my computer's language to English, I can't install it. Also, there doesn't seem to be anything unusual in the installation directory.