2025-10-14 12:17 AM
Hi!
I am trying to connect X-NUCLEO iks01A3 to NUCLEO STM32F411. We can see that X-NUCLEO iks01A3 is compatible with NUCLEO F401RE, NUCLEO L053R8, NUCLEO L152RE or NUCLEO L476RG. I checked up the pinout of NUCLEO STM32F411 and NUCLEO F401RE and have found out that it is the same. Moreover, pins that are responsible for I2C are the same too. I don`t use UNICLEO-GUI to get a data from all the sensors that are placed on X-NUCLEO iks01A3 board, but I want to use only the initialization code generated by CUBE MX and the HAL function