2026-05-12 12:48 AM - last edited on 2026-05-12 1:58 AM by Andrew Neil
When using the IOC file in the attachment to generate code with an operating system, MDK-ARM V5.32 is selected. It is found that the directory ..\Middlewares\Third_Party\FreeRTOS\Source\portable\GCC is missing, resulting in compilation failure in Keil.
2026-05-12 1:19 AM
Hello @XUFEI
I am checking this behavior. I will get back to you ASAP.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.