cancel
Showing results for 
Search instead for 
Did you mean: 

Missing global variables which are not arrays when loading axf file.

VOlet.1
Associate II

I am using keil compiler and loading the .axf file.

Other than global variable which are arrays no other global variables are visible in the variable list for selection.

What i am missing here?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Thierry
Senior

@VOlet.1​  Please be informed that the version numbers are now aligned between ST site and "about" window from the tool itself.

Thanks again for having raised the mismatch.

View solution in original post

10 REPLIES 10
stephane.legargeant
ST Employee

Hello VOlet.1 Do you mean that you don't have any variable listed when you load the file. Or do you have some variables, but others are missing ?

VOlet.1
Associate II

Hi,

Only few variables are displayed (Most variables are missing).

Interestingly, I see only arrays in the list.

No other variables (apart from arrays) are listed in the window.

Thierry
Senior

Dear VOlet.1,

Could you share your axf file such as we can look at what is going wrong ?

Thanks

VOlet.1
Associate II

Hi,

Is it possible that i email/send file directly without posting publicly?

Thierry
Senior

Dear VOlet.1,

Thanks for having shared the axf file by private message.

From what I saw in your axf file, all the non decoded variables are coming from classes in .cpp files.

Unfortunately, and as mentioned in this thread , the C++ is currently not supported (or very partially like for arrays in your case) by STM32CubeMonitor parser.

VOlet.1
Associate II

Hi Thierry,

Thanks for checking on this and duly noted.

I hope this is addressed in upcoming releases.

Speaking of version numbers i couldn't find any option through which i could check which version of cube monitor i am running.

Any way of finding this out from GUI?

Thierry
Senior

Dear VOlet.1,

For version numbers, you should be able to check it by opening "About STM32CubeMonitor" popup window from hamburger menu.

VOlet.1
Associate II

Sorry i missed that, thanks.

But do note that the version numbers listed on the site doesn't match with the number on the app.

And thank you for the quick and helpful replies!

Thierry
Senior

You are welcome. Thanks for highlighting the version mismatch, the one from about window is the correct one :)