cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 2.0.0 on macOS Tahoe 26.2 (Apple Silicon M4): text selection not visible

CColo.2
Associate III

Ambiente

Sistema operativo Mac Tahoe 26.2 (25C56)

Apple Silicon M4

STM32CubeIDE 2.0.0 (x86_64, ejecutándose bajo Rosetta 2)

Asunto

STM32CubeIDE se inicia correctamente, pero la selección de texto no se representa visualmente en ninguna parte del IDE (editor, consola, vistas).

La selección del mouse y del teclado no muestra ningún resaltado.

Copiar/pegar funciona normalmente , lo que indica que la selección existe internamente pero no se muestra.

La selección de texto funciona correctamente en otras aplicaciones de macOS.

Pasos para reproducir

1. Inicie STM32CubeIDE en Rosetta:

arch -x86_64 /Aplicaciones/ST/STM32CubeIDE.app/Contenidos/MacOS/STM32CubeIDE

2.Abra cualquier archivo fuente.

3.Intenta seleccionar texto.

Solución de problemas realizados

Instalación de Rosetta 2 verificada.

Restablecer preferencias y espacio de trabajo.

Espacio de trabajo limpio probado.

 Deshabilitado el renderizado SWT Metal/gestos a través de opciones .ini.

El problema persiste.

21 REPLIES 21

I can advise to do a rework. its easy and solves issues on 26.2 Tahoe for 1.19. The link is 1 post above

Hello @FOFI 

Our development team remains committed to customers and collaborators satisfaction and is engaged in aligning the STM32CubeIDE with macOS Tahoe 26.2.

We will share further information as it becomes available.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks, I assume this does not work for version 2.0? I have tried it twice and upon start using clean I get an error log containing 

Caused by: java.lang.ClassNotFoundException: An error occurred while automatically activating bundle org.eclipse.ui.workbench (388).

Hello,

I didn't check 2.0 but other report its working. I had errors lunching as well. how do you open the LIST file ? with Text.edit ? if so - check the pasted name with the file name. For some reaspon it can autocorrect : " , " to " _ " or opposite 

I already confirmed that wasn’t the issue. I tried it a second time using VS Code, since I know how unpredictable TextEdit can be. I’ve given up for now and am currently downgrading my machine to Sequoia, as I’m also not satisfied with the current design choice.

Sorry to hear that. On a side note, can you confirm if you can flash your MCU with V3minie dongle on Tahoe ? (If you use V3minie of course) 

I do not have the V3minie. 

Arete
Associate II

Still looking for an update, patch or workaround.

The fix exist. Need to manually patch Eclipse files. 

Tony2024
Associate II

I just ran into the same problem. MacOS was updated and now can't see selected text.

IDE 2.1.1

MacOS 26.4.1

Apple M4 Pro