cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with ST VSCode STM32 extension.

SidPrice
Associate III

Hello, I have been using the VSCode STM32 extension on my project for some time and it has been working well. Today, I was doing some major refactoring of some of the code, and this required deleting one of the files no longer required. Unfortunately, the extension did not recognize the file had been deleted and the build failed when it could no longer find the file.

I fixed the issue by going back to STM32CubeIDE and refreshing the project. Then I returned to VSCode, opened my project and performed an "Import local project."

While this fixed my issue, it seems the extension should be able to cope with a file being deleted without having to return to STM32CubeIDE.

Did I miss some other option in the extension?

Sid

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

The extension isn't made by ST. Perhaps report it on the project's page with enough information to replicate the issue.

https://github.com/bmd-studio/stm32-for-vscode

 

If you feel a post has answered your question, please click "Accept as Solution".
SidPrice
Associate III

@TDK The copyright shown by the extension is ST MicroElectronics, with a link to st.com!

Sid

Oh, looks like there is an official one now. There wasn't for a long time. Sorry for the noise.

https://community.st.com/t5/other-tools-mcus/vscode-for-stm32-extension-1-0-0-released/td-p/143795

 

If you feel a post has answered your question, please click "Accept as Solution".