2024-11-05 6:34 AM
IDE hangs after collapsing ( minimizing window) and expanding (maximizing). Or after Alt + Tab. From time to time.
"File -> Restart" only helps.
I don't know how to fix this. Please, help.
Tried to reinstall - the same situation.
IDE uses internal Java: java.version=17.0.11
As system Java versions, I have v.18, 21, 22 (checked via "update-alternatives --config java" command)
Just have an idea to try to switch from internal to system version of Java, but did not find how it can be done.
My config:
Laptop Dell Vostro 3520
Ubuntu 22.04.4
2024-11-05 6:59 AM
2024-11-06 12:27 AM
Hello @VK.17
Have you tried the CubeIDE 1.16.1 version? Can you check if the behavior still occurred?
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-06 1:22 AM
Yes, the same behavior.
2025-12-15 8:35 AM
I'm using the version 2.0.0 and the same behavior. The problem persists.
Arch Linux, fully updated, using Wayland.