cancel
Showing results for 
Search instead for 
Did you mean: 

I cannot install st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.

YDOOY.1
Associate II

Hi

I install st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exe first in my PC.

But I excute the file, then display follow message and cannot install.

what I have mistake ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Markus GIRDLAND
ST Employee

To start off I would double check a few things:

  • Proper permissions to execute the file
  • Download of the file from the website was successful, the md5 checksum should be: 040ae6096a19e6603280966eb0789dff
  • No anti-virus and/or firewall interruption
  • The computer is 64-bit

If all of those are checked. Please try to place the installer in a short path and then launch it, for example:

C:\ST\st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exe

Let me know if the problem persists after trying those things.

View solution in original post

3 REPLIES 3
YDOOY.1
Associate II

The image is not uploaded.

Error Message is that

NSIS Error

Error Launching installer

OK

Markus GIRDLAND
ST Employee

To start off I would double check a few things:

  • Proper permissions to execute the file
  • Download of the file from the website was successful, the md5 checksum should be: 040ae6096a19e6603280966eb0789dff
  • No anti-virus and/or firewall interruption
  • The computer is 64-bit

If all of those are checked. Please try to place the installer in a short path and then launch it, for example:

C:\ST\st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exe

Let me know if the problem persists after trying those things.

YDOOY.1
Associate II

Dear Markus

I checked downloaded file, and install successfully.

Thanks a lot.