cancel
Showing results for 
Search instead for 
Did you mean: 

Can't compile X-Cube-Cellular TCP_Echo_Client example

GBeto.1
Associate II

Hi,

I'm running STM32Cube 1.11.2 under Ubuntu 22.04

While I can compile the TCP_Echo_Client_PPP example with no issue, I can't do the same with TCP_Echo_Client.

The compilation issue is the tx_thread_schedule.s has undefined references to _tx_thread_secure_stack_context_save, _tx_thread_secure_stack_context_restore, _tx_thread_secure_mode_stack_allocate, _tx_thread_secure_mode_stack_free and _tx_thread_secure_mode_stack_initialize

This issue is systematic, including trying with a fresh new workspace.

Thank you for your help,

Guillaume

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ronan GABOU
ST Employee

Hello,

In the IDE project in the following directory:

Middlewares\ST\threadx\ports\cortex_m33\gnu\src\

replace the 9 files .s with .S

It should solve you compilation issue.

Ronan,

View solution in original post

5 REPLIES 5
GBeto.1
Associate II

I finally succeded but I'm not sure this is the right answer :

  • in Middlewares/ThreadX/ports/cortex_m33/gnu/src I only have *.S files ('S' is uppercase)
  • when compiling it generates some the same filenames, but with *.s extension (lowercase)
  • those files do not have same content, and moreover do not contains the #if to avoid compiling the 'secure' part
  • I did simply override those .s files with originals .S files

=> compiles and seems to run OK

Maybe this is a Linux only issue ?

Ronan GABOU
ST Employee

Hello,

In the IDE project in the following directory:

Middlewares\ST\threadx\ports\cortex_m33\gnu\src\

replace the 9 files .s with .S

It should solve you compilation issue.

Ronan,

It's the opposite : I have to rename de 9 files .S with .s :D

But thank you for the confirmation.

Ronan GABOU
ST Employee

If you modify in the IDE as I suggested you must change .s in .S (because the files on disk are .S)

If you prefer change on the disk you can change .S in .s but other projects won't work anymore.

So it is up to you to decide the preferred correction.

Ronan,

Oh yes got it, thanks a lot.