2024-11-18 3:14 PM
I encountered an STLINK connection error when developing with VSCODE + STM32 VSCODE EXTENSION using the NUCLEO-H503RB MR2 board.(MR1 is no problem)
#Development Tool 1: STM32CubeMX 6.12.1
#Development Tool 3: Visual Studio Code
#Extension: STM32 VSCode Extension Pack
#Development Tool 4: STM32Cube CLT 1.16.0
However, when installing STM32Cube CLT, I did not install STLINK. Instead, I separately installed Development Tool 2: STM32IDE 1.16.1 and installed STLINK, which resulted in normal operation. Since I don't actually use the IDE, it would ideally be better to install STLINK when installing CLT. Is there a difference in the STLINK version or other factors between IDE and CLT?
I will proceed with development using this environment, but since I suspect it might be a tool-related issue, I wanted to report it.
2024-12-10 5:59 AM
Hi @dai82s
Seems an stlink FW update issue, please upgrade your stlink FW in the concerned board and try again