cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to find STM32MP157D-DK1 board definition

etheory
Senior II

Hi there!

 

I just purchased an STM32MP157D-DK1 discovery board, and noticed that in STM32CubeIDE there are no definition files for this model, only a subset of the other MP1 discovery boards (but curiously not all of them).

 

Is this product unsupported by ST or can I obtain board definition files from elsewhere?

 

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @etheory​ ,

This is a known limitation :

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note#STM32CubeMX_2

Warning: To generate an device tree for new Boards STM32MP157D-DK1, STM32MP157D-EV1, please select respectively the ST boards project STM32MP157F-DK2, STM32MP157F-EV1. The generated device trees will work but with some probe errors on Crypto, Display DSI, Wifi, BT linux drivers for STM32MP157D-DK1 board and on Crypto Linux driver for STM32MP157D-EV1.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @etheory​ ,

This is a known limitation :

https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note#STM32CubeMX_2

Warning: To generate an device tree for new Boards STM32MP157D-DK1, STM32MP157D-EV1, please select respectively the ST boards project STM32MP157F-DK2, STM32MP157F-EV1. The generated device trees will work but with some probe errors on Crypto, Display DSI, Wifi, BT linux drivers for STM32MP157D-DK1 board and on Crypto Linux driver for STM32MP157D-EV1.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Khouloud ZEMMELI
ST Employee

Hello @etheory​ 

There's a plan to support the STM32MP157D-DK1 board and the other missed boards soon for both CubeMX and CubeIDE (6.3.0 and 1.7.0).

You can find in this link all documents about the STM32MP157D-DK1.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your feedback, Khouloud

Hello @etheory​ ,

I'm back again to inform you that STM32MP157D-DK1 board is now supported, you can use the latest CubeMX version available on site :)

Khouloud

Thank you @Khouloud ZEMMELI​ much appreciated for the update.

Does this also include STM32CubeIDE?

Yes! Same for the latest CubeIDE version, also available on site.

Always welcome @etheory​  :) Khouloud