STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

cube programmer sd card image download- STM32MP1

These are log i got during download, any clueSTM32_Programmer_CLI -c port=usb1 -tm 20000 -w flashlayout_mp1som-image/FlashLayout_sdcard_mp1som-mystm32mp1-basic.tsv    -------------------------------------------------------------------                ...

Ara.1 by Senior
  • 3293 Views
  • 7 replies
  • 0 kudos

SSH Connection to STM32CUBEIDE

Hi,How can I connect to STM32MPU via SSH from inside STM32CUBEIDE.?? Is there a way we can do that?This really helps in live debug of things.Alternatively is there a way I can live debug an application running on A7?

NPal.2 by Senior
  • 2416 Views
  • 3 replies
  • 0 kudos

stm32mp1 uart noise rx

Hi All,i am using stm32mp1 cpu,, recently i m facing floating rx issue on debug uart, with physical debug cable , i could default state of RX lines were pull up, and when i remove the cable, the RX lines is floating and its voltage fluctuates between...

Ara.1 by Senior
  • 3693 Views
  • 5 replies
  • 0 kudos

Resolved! How to create a debug configuration in STM32CubeIDE to debug Linux Kernel on STM32MP157A-DK1?

Hi,I'm trying to create a debug configuration in STM32CubeIDE to debug Linux Kernel but I can't find any related article about the issue. I want to use gdb with ST-LINK (OpenOCD) as JTAG device to debug the Kernel that I have already compiled.Any sug...

LRava.1 by Associate
  • 1609 Views
  • 1 replies
  • 0 kudos