2024-09-27 6:11 AM
Ok, good to know it is a known issue. And no problem with it.
What can I do then in order to proceed ?
Are there other files missing ?
How can I complete the installation and make sure eveyrthing is there ?
2024-09-27 5:03 PM
Hello,
Just so you know, I just searched on your forum if we had not already encountered this problem of missing "freertos_mpool.h" file.
I found this thread here. Problems with stm32f103zet6 using stm2cubeIDE to build freertos projects
Your colleague there suggests going back to version 1 of CMSIS.
I don't see any problem, that's what I did.
And now it works ! Everything compiles perfectly until the end without error or warning.
I now move on to the next step which consists of downloading the binary code normally obtained to the "STM32F107-VCT6" chip at my disposal.
Thank you for the speed of your answers.
I will not hesitate to come back to you if I encounter other problems that I cannot solve.
Kind regards,
--
MDe / Belgium