Skip to main content
Associate III
August 13, 2024
Solved

Can't boot the EMMC with a USB on the STM32MP257F-EV1

  • August 13, 2024
  • 2 replies
  • 1339 views

Hello,

 

I am trying to boot an EMMC with a USB on a STM32MP257F-EV1 Development board and am having troubles. I set the boot pins to what is said in the data sheet for EMMC (That being Boot2 is set to 1 and the rest 0) The USB is no longer an option to connect to. (For reference I am trying to follow this wiki article: Populate the target and boot the image - stm32mpu but only using the EMMC instead of the SD Card). Any help would be greatly appreciated. Thanks!

This topic has been closed for replies.
Best answer by Carson

Hi Erwan, 

 

I figured out that most my problems stemmed from supplying power from the ST link and not through the Jack. 

 

Thanks.

2 replies

Erwan SZYMANSKI
ST Technical Moderator
August 14, 2024

Hello @Carson ,
Can you follow this article and tell me back if you still have troubles ? https://wiki.st.com/stm32mpu/wiki/STM32MP25_Evaluation_boards_-_Starter_Package

Do not forget to connect the USB_DRD to your host PC, to verify that your CubeProgrammer is the right version (2.17) and to take the eMMC flashlayout instead of the default SDcard one.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CarsonAuthorBest answer
Associate III
September 18, 2024

Hi Erwan, 

 

I figured out that most my problems stemmed from supplying power from the ST link and not through the Jack. 

 

Thanks.