2024-02-02 1:32 AM
i have download prebuild image
en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz
it working fine on my stm32mp135f-dk EVK.
i want to add docker in it so need the build process of yocto image.
Kindly guide me how to do it.
Solved! Go to Solution.
2024-02-05 2:38 AM
Hi @Subhashzimetrics ,
Please have a look to our wiki documentation STM32MP135x-DK - software distributions - stm32mpu
Hope it help,
Olivier
2024-02-05 2:38 AM
Hi @Subhashzimetrics ,
Please have a look to our wiki documentation STM32MP135x-DK - software distributions - stm32mpu
Hope it help,
Olivier
2024-02-21 9:49 PM
@Olivier GALLIEN thanks for support.
During build process we need to remove "seccomp" this
just remove `REQUIRED_DISTRO_FEATURES = "seccomp"` from `meta/recipes-support/libseccomp/libseccomp_2.5.4.bb
Is any process to enable "seccomp" in docker
2024-02-21 11:47 PM
What do you mean by "we need to remove "seccomp""
Should i understand this recipes generate an error in docker ?
If yes please attached error log.
Thx
Olivier
2024-02-22 10:31 PM
@Olivier GALLIEN please find the logs
pc-lab@pclab-NUC11PAHi7:~/stm32mp1_distribution_package/build-openstlinuxweston-stm32mp13-disco$ bitbake st-image-weston
NOTE: Started PRServer with DBfile: /home/pc-lab/stm32mp1_distribution_package/build-openstlinuxweston-stm32mp13-disco/cache/prserv.sqlite3, Address: 127.0.0.1:44547, PID: 3529147
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:00
Loaded 5052 entries from dependency cache.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:00:00
Parsing of 3212 .bb files complete (3211 cached, 1 parsed). 5052 targets, 593 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing PROVIDES 'libseccomp' (but /home/pc-lab/stm32mp1_distribution_package/layers/meta-virtualization/recipes-containers/docker/docker-ce_git.bb DEPENDS on or otherwise requires it)
libseccomp was skipped: missing required distro feature 'seccomp' (not in DISTRO_FEATURES)
NOTE: Runtime target 'docker' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['docker', 'libseccomp']
ERROR: Required build target 'st-image-weston' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-image-weston', 'docker', 'libseccomp']