STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP153C SSP workflow

I am developing a device with the STM23MP153C and plan to implement secure boot, but I don't fully understand the SSP workflow and have a few questions.1. The STM32CubeProgrammer documentation says that the -ssp command can be executed both with HSM ...

axel101 by Associate III
  • 1560 Views
  • 1 replies
  • 0 kudos

Resolved! Qt SDK build failed with turorial

Hey, I'm following the Distribution Package tutorial, specifically the QT image and SDK with EGLFS tutorial: wiki  I did build the Qt image with     bitbake st-example-image-qt     but building the SDK with     bitbake st-example-image-qt -c populate...

oli1 by Associate II
  • 4341 Views
  • 4 replies
  • 2 kudos

STM32MP157F DDR Caching/Organization

Hello, we are currently working with the STM32MP157F-DK2 evaluation board. We have a couple questions regarding the DDR setup on the board. First, when accessing DDR memory, is there any level of CPU caching occurring, or can the memory region have c...

Bit Mapping.png
heelsec by Associate
  • 2189 Views
  • 0 replies
  • 0 kudos

switch off/on pmic

HI,Voici mon problème, Sur ma carte éléctronique, j'ulise un stm32mp15 ave le pmic de ST. J'utilise la broche LD02 du pmic pour allimenter un récépteur GPS (relié sur l'uart 7) que j'aimerai pouvoir couper/allumer (depuis le user space) pour des ques...

ABouc.1 by Associate
  • 1972 Views
  • 2 replies
  • 0 kudos

Resolved! USB HID doesn't work without hub

Hi, when I inserted keyboard/mouse to USB host port, nothing happened (log console) and this even cause usb host stop working then.But when I inserted keyboard/mouse to a hub and connect this hub to usb host port, everything working fine.The problem ...

Dat Tran by Senior II
  • 3873 Views
  • 2 replies
  • 1 kudos