cancel
Showing results for 
Search instead for 
Did you mean: 

Setting up CubeIDE for RA-08/ASM6601?

SDavi.6
Associate

So I have seen several people say they used the Cube IDE to program the RA-08 from AI-Thinker. They say it was super easy and I love CubeIDE. but for the life of me I don't understand how they did it. Please help?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome,@SDavi.6​, to the community!

Well, even if you cite the sources, I question their statement because the STM32CubeIDE only supports STM32 from STMicroelectronics. However, the RA-08 module from Ai-Thinker uses the ASR6601 chip from the Chinese manufacturer ASR, as you can read in its description, which has absolutely nothing to do with STM32:

Ra-08-Kit is a LoRaWAN development board designed and developed by Shenzhen Ai-Thinker Technology Co., Ltd. [...]

The chip ASR6601 on the development board is a general-purpose LPWAN wireless communication SoC that integrates an RF transceiver, a modem and a 32-bit RISC MCU. The MCU adopts ARM core, and the operating frequency can reach 48MHz. [...]

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome,@SDavi.6​, to the community!

Well, even if you cite the sources, I question their statement because the STM32CubeIDE only supports STM32 from STMicroelectronics. However, the RA-08 module from Ai-Thinker uses the ASR6601 chip from the Chinese manufacturer ASR, as you can read in its description, which has absolutely nothing to do with STM32:

Ra-08-Kit is a LoRaWAN development board designed and developed by Shenzhen Ai-Thinker Technology Co., Ltd. [...]

The chip ASR6601 on the development board is a general-purpose LPWAN wireless communication SoC that integrates an RF transceiver, a modem and a 32-bit RISC MCU. The MCU adopts ARM core, and the operating frequency can reach 48MHz. [...]

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.