cancel
Showing results for 
Search instead for 
Did you mean: 

Python Missing Modules on STM32MP1 OpenSTLinux

MakerMelissa
Associate II

I have an STM32MP1-DK2 and have tried to install pip using several python mechanisms, but there are missing modules. The notable ones that I found missing are runpy and xmlrpc. Even when I go into python and type help() it spits out an error about pydoc missing. All available python packages have been installed via apt-get install.

I'm wondering do I have a bad image or is there a way to get these built-in packages?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

This did not work with version 1.2 that came on the SD Card that came with the STM32MP1, but on the 2.0 version I flashed, after running apt-get update, it worked!