2022-07-07 1:03 AM
What kind of encryption performance can we expect from the cryptoprocessor? SoC is STM32MP157 with kernel 5.10. Currently we get:
root@host:~# cryptsetup benchmark
# Tests are approximate using memory only (no storage IO).
PBKDF2-sha1 57186 iterations per second for 256-bit key
PBKDF2-sha256 84453 iterations per second for 256-bit key
PBKDF2-sha512 52512 iterations per second for 256-bit key
PBKDF2-ripemd160 47558 iterations per second for 256-bit key
PBKDF2-whirlpool 11425 iterations per second for 256-bit key
argon2i 4 iterations, 31804 memory, 4 parallel threads (CPUs) for 256-bit key (requested 2000 ms time)
argon2id 4 iterations, 32529 memory, 4 parallel threads (CPUs) for 256-bit key (requested 2000 ms time)
[ 199.200180] sched: RT throttling activated
# Algorithm | Key | Encryption | Decryption
aes-cbc 128b 4.1 MiB/s 4.1 MiB/s
serpent-cbc 128b N/A N/A
twofish-cbc 128b N/A N/A
aes-cbc 256b 4.1 MiB/s 4.1 MiB/s
serpent-cbc 256b N/A N/A
twofish-cbc 256b N/A N/A
aes-xts 256b 4.0 MiB/s 4.1 MiB/s
serpent-xts 256b N/A N/A
twofish-xts 256b N/A N/A
aes-xts 512b 4.1 MiB/s 4.0 MiB/s
serpent-xts 512b N/A N/A
twofish-xts 512b N/A N/A
When using the CPU instead of the cryptoprocessor we get:
root@host:~# cryptsetup benchmark
# Tests are approximate using memory only (no storage IO).
PBKDF2-sha1 57893 iterations per second for 256-bit key
PBKDF2-sha256 84128 iterations per second for 256-bit key
PBKDF2-sha512 52597 iterations per second for 256-bit key
PBKDF2-ripemd160 47766 iterations per second for 256-bit key
PBKDF2-whirlpool 11397 iterations per second for 256-bit key
argon2i 4 iterations, 32573 memory, 4 parallel threads (CPUs) for 256-bit key (requested 2000 ms time)
argon2id 4 iterations, 32866 memory, 4 parallel threads (CPUs) for 256-bit key (requested 2000 ms time)
# Algorithm | Key | Encryption | Decryption
aes-cbc 128b 12.5 MiB/s 14.4 MiB/s
serpent-cbc 128b N/A N/A
twofish-cbc 128b N/A N/A
aes-cbc 256b 9.9 MiB/s 10.5 MiB/s
serpent-cbc 256b N/A N/A
twofish-cbc 256b N/A N/A
aes-xts 256b 15.9 MiB/s 13.9 MiB/s
serpent-xts 256b N/A N/A
twofish-xts 256b N/A N/A
aes-xts 512b 12.3 MiB/s 10.7 MiB/s
serpent-xts 512b N/A N/A
twofish-xts 512b N/A N/A
The kernel message
[ 199.200180] sched: RT throttling activated
during the cryptoprocessor benchmark is strange. It does not happen, when doing file transfers on the encrypted target, though.
Can anyone from ST please evaluate these values? @Community member @Sara BEN HADJ YAHYA
2022-07-10 10:00 PM
Hi @johnnyc
Your results looks inline with what have been already reported and analyze in some other thread like this one :
https://community.st.com/s/question/0D53W00001JUAMJSA5/issues-with-crypto-ip-core
Its conclusion is still valid :
ST policy about Linux is to rely on Linux framework + HW driver adaptations to these framework to better upstream an overall solution maintained by the community (and therefore giving more sustainability of ST solution for customers).
Doing this for Cryptodev framework shows the results you highlight here: for some cases, performances are very low compared to full cpu and with the same cpu load ....
A study is ongoing to check what could be done to improve this (depending on HW capability and SW adaptation required on top of HW drivers) but there is no short term solution.
Olivier
2024-03-21 3:39 AM