cancel
Showing results for 
Search instead for 
Did you mean: 

Level of Support for custom Operating System?

JAppe.1
Associate II

Hello,

I'm writing to inquire if there is documentation/support for developing non-linux operating systems using the STM32 MPU discovery kits. So far I've only found Cube support and documentation for ST's custom linux distro. Obviously, a processor being a processor, it can run anything I put in the ROM. But I'd like to be able to utilize some of the development tools that these boards are supposed to support to make the development/debugging experience easier.

I'm using a STM32MP157D-DK1, in case that makes any major difference.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan SZYMANSKI
ST Employee

Hello @JAppe.1​ ,

Unfortunately, the only OS that ST supports on MPU side is OpenSTLinux (which is our specific Linux distribution). You are right, there are various way to use and program a microprocessor, but ST specific Linux is the only one supported by our teams.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.