Skip to main content
SGaut
Associate
August 21, 2019
Solved

I am reading ITM traces by SWO Printf style debugging. Can this debug information be read by a UART receiver on a FPGA ?

  • August 21, 2019
  • 3 replies
  • 1219 views

..

This topic has been closed for replies.
Best answer by AntonioST

I do not see issues here. The SWO pin can be programmed for one between two encoding: UART or Manchester.

The data sent out in UART mode can be read by any UART receiver (pay attention to the voltage level, so you need a UART receiver at 3.3V) once you have set the proper baudrate and parity.

I never used the Manchester encoding, due to lack of proper receiver. But in a FPGA implementation the Manchester receiver could be more interesting than the UART one; the bit clock can be extracted directly from the data-stream and the RTL implementation could be far smaller than a full UART.

3 replies

Tesla DeLorean
Guru
August 22, 2019

I'd assume so, one could presumably code the FPGA to handle other protocols too.

https://developer.arm.com/docs/ddi0314/latest/serial-wire-output/swo-trace-port/physical-pin-protocol

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AntonioST
AntonioSTBest answer
ST Employee
August 22, 2019

I do not see issues here. The SWO pin can be programmed for one between two encoding: UART or Manchester.

The data sent out in UART mode can be read by any UART receiver (pay attention to the voltage level, so you need a UART receiver at 3.3V) once you have set the proper baudrate and parity.

I never used the Manchester encoding, due to lack of proper receiver. But in a FPGA implementation the Manchester receiver could be more interesting than the UART one; the bit clock can be extracted directly from the data-stream and the RTL implementation could be far smaller than a full UART.

SGaut
SGautAuthor
Associate
August 23, 2019

Thank you for your inputs .