How to use DDR3 with Cortex-A7 (STM32MP157C-DK2 - C++ project)?
- January 11, 2021
- 3 replies
- 1142 views
Good morning,
I'm working on a C++ project to collect data from a peripheral sensor using the STM32MP157C-DK2.
The estimated amount of data is at least 100 MB, so I have to use the DDR3 to store these data and then trasmit them over Ethernet using at the moment ONLY Cortex-A7 (no M4).
The project is write in C++ language and NOT using CubeMX, so I'm asking how can I activate and use the DDR3.
I've read some tutorials/documents from various sources:
# https://www.st.com/en/microcontrollers-microprocessors/stm32mp157.html#documentation
# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example
and consequently I wrote the code (you will find it here attached with the dts in the card partition called "bootfs"), but I always receive the cout message "Mapping param failed.".
What I've to modify in the main code and, eventually, how/where can I add/modify the missing dts data to the MP1?