2023-06-18 10:18 PM - edited 2023-06-18 10:22 PM
Hello,
I am a newcomer to embedded systems. I have a STM32MP157D-DK1 and I'm planning to develop some python applications to run on the A7 processor. I am encountering some issues.
1. I created a simple web application using Python on Ubuntu. (python module: Flask)
2. I confirmed that it can be executed successfully.
3. I bundled it into a single executable file using pyinstaller (PC $> pyinstaller app.py --onefile).
4. I verified that the executable file can be used properly.
5. I transferred the file to an STM32 (starter kit).
6. When I tried to execute the file, an error occurred.
Error Message:
./app: line 1: syntax error: unexpected ")"
Other experiments:
I try to execute python source code directly on STM32, there is no problem.
I try to bundle python code into a single executable on STM32, but can't install pyinstaller. (pip3 install pyinstaller)
Thanks for your support,
Ken.
2023-06-26 5:44 AM - edited 2023-06-26 6:01 AM
Hi @Ken_102633
The app you created with pyinstaller from your PC running ubuntu is compiled for an architecture compatible with your PC (most probably x86_64). However, STM32MP15 boards rely on a ARM architecture hence can't run x86_64 app. That explains the error you got in your 6th step.
Then, installing pyinstaller from pip3 shows errors as some build dependencies are not available such as a gcc toolchain. To bypass these dependencies, you need to build your own distribution and setup your own repository (please refer to https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#How_to_activate_a_local_package_repository )
Once your repository is activated, install the package group core-buildessential:
root@stm32mp1:~# apt-get update
root@stm32mp1:~# apt-get install packagegroup-core-buildessential
# EDITED SECTION BELOW
root@stm32mp1:~# apt-get install ldd
You can now install pyinstaller with the following command:
root@stm32mp1:~# env PYI_STATIC_ZLIB=1 pip3 install pyinstaller
Then try to build your app.
Best regards,
--JM
2024-01-02 2:01 AM
Thank you so much @Jean-Marc B , the steps listed here helped to install and work with pyinstaller on stm device!
2024-11-27 5:13 AM
Firstly I builded the latest distribution package to kit. then-
I have done steps according to this link (https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#How_to_activate_a_local_package_repository)
1.
cd [your STM32MP2 Distribution path]/build-openstlinuxweston-stm32mp15-disco bitbake package-index
2.
cd [your STM32MP2 Distribution path]/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/deb python3 -m http.server &
In this path which is provided i have seen that in my distribution build only 3 of files are their and they are all, cortexa7t2hf-neon-vfpv4 and stm32mp15_disco.
3.on board(kit)
echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
in this i have added ip of host pc.
but when i tried the deb things for the board it was not able to fetch
Then as you mentioned in this thread to do:
root@stm32mp1:~# apt-get update root@stm32mp1:~# apt-get install packagegroup-core-buildessential # EDITED SECTION BELOW root@stm32mp1:~# apt-get install ldd
after that it is not able to install the core build essetial
it shows the error that it is not able to locate the build essetial
ldd where installed .
atlast i was not able to install pyinstaller
2024-11-27 9:42 PM
Hii @Jean-Marc B
Please help me to resolve the issue .
As i mentioned in my above post.
Your help would be great.
2024-11-27 11:37 PM
Hi @Mohanv
From your linux PC, check the packagegroup-core-buildessential package is available in your local deb directory:
[your STM32MP2 Distribution path]/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/deb
by typing the following command:
$ find . -name "packagegroup-core-buildessential_*.deb" -print
If the package is missing, you need to build it with the command and redo the package indexes:
$ bitbake packagegroup-core-buildessential
$ bitbake package-index
From your board, update your APT configuration and check the package is available:
root@stm32mp1:~# apt-get update
root@stm32mp1:~# apt-cache policy packagegroup-core-buildessential
root@stm32mp1:~# apt-get update
root@stm32mp1:~# apt-cache policy packagegroup-core-buildessential
If yes, then perform the installation:
root@stm32mp1:~# apt-get install packagegroup-core-buildessential
Best regards,
--JM
2024-11-28 6:55 AM
Hii @Jean-Marc B
Thank you for the response .
I have done the steps as you suggested, I was able build and fetch the packagegroup-core-buildessential for my board .
but while getting the apt update
I got this error
so when I viewed in my host pc for deb files in the build path
so i changed the filename for getting from the server of host pc
echo "deb [trusted=yes] http://<IP>:8000/stm32mp15_disco /" > /etc/apt/sources.list.d/my_custom.list
and I also saw that the cortexa7hf-neon-vfpv4 is missing in my built
Still I went ahead try to install pyinstaller but I ran into this error
2024-11-28 11:46 PM
Hi @Mohanv
The error says the libz library is missing.
Try to build it if not present in your repo (bitbake zlib1) or install it with apt-get install zlib1
Best regards,
--JM
2024-11-29 6:03 AM
Hi @Jean-Marc B
and thank you for your quick response.
I was not able to build the zlib1 and was also not able to install it. with error
and my main concern is to install pyinstaller.
so is this zlib is needed to do that .
I have doubt when you said that to rearrange the index in above suggestion , so should we not need to flash it to the kit
Guide me step by step to get proper files so i can install pyinstaller properly and as i mentioned above message you can see that it have error with pyproject.toml time.
2024-11-29 7:07 AM
Hi @Mohanv
The bitbake error message shows the right recipe to be called: zlib.
So, you need to build zlib then update your package index. That would give:
$ bitbake zlib
$ bitbake package-index
Then refresh your APT configuration and install the zlib package from your ST board:
# apt-get update
# apt-get install zlib
Best regards,
--JM