2022-09-28 1:56 AM
Hi,
I'm using stm32mp153c and I managed to start M4 code after the SPL initialization and before U-BOOT. All initializations work fine except for the MX_OPENAMP_Init.
I see that if I start the code after SPL the variable of num_of_vrings (that is equal to the define VRING_COUNT 2) is 0. Whereas if I start the M4 code directly from linux the variable is set to 2 and the OPENAMP initialization works.
I tried to set a delay of 1 minute before the IPCC and OPENAMP initializations (in order to wait for LINUX to enable virt_uart and rpmsg_sdb devices) but the OPENAMP initialization still failed.
Any suggestions?
Thanks in advance.
Best regards,
Andrea
2022-11-22 1:17 AM
Hello,
Look like that you don't load the .resource_table section in memory, or that the SPL does not provide the address to the Linux.
1 ) Do you fill the backup/tamp registers to provide the M4 state and resource table address information to the Linux?
cf U-boot code here:https://elixir.bootlin.com/u-boot/latest/source/drivers/remoteproc/stm32_copro.c#L149
2) if done first check in Linux console that the remoteproc is in "detached" state
root@stm32mp15-disco-oss:~# cat /sys/class/remoteproc/remoteproc0/state
detached3) attach it
root@stm32mp15-disco-oss:~# echo start >/sys/class/remoteproc/remoteproc0/state
root@stm32mp15-disco-oss:~# cat /sys/class/remoteproc/remoteproc0/state
attached
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.