2022-04-26 1:05 PM
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!adc_measurement: single shot failed for adc@0[18]!
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
Boot over usb0!
DSI version 0x0 not supported
Invalid or missing layout file.DFU alt info setting: doneWe can successfully load the StarterPackage FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv, but when we try creating from Developer Package, we get this error.
Our board has a STM32MP151CAC. We have been testing on the STM32MP157F-DEV2, on which there has been no problem.
Is there a default for booting over USB, and not the SD?
Thanks in advance,
George
2022-04-29 8:25 AM
Hi @GeorgeR ,
I understand trace you provide come from console while flashing with CubeProg right ?
>>Our board has a STM32MP151CAC. We have been testing on the STM32MP157F-DEV2, on which >> there has been no problem.
MP151C and MP157F can not boot with same BSP settings. Device Tree have to be adapted.
Can you please provide :
Olivier