2020-09-06 9:43 PM
My device tree configuration
{
spdif_out: spdif-out {
#sound-dai-cells = <0>;
compatible = "linux,spdif-dit";
status = "okay";
spdif_out_port: port {
spdif_out_endpoint: endpoint {
remote-endpoint = <&sai4a_endpoint>;
};
};
};
spdif_in: spdif-in {
#sound-dai-cells = <0>;
compatible = "linux,spdif-dir";
status = "okay";
spdif_in_port: port {
spdif_in_endpoint: endpoint {
remote-endpoint = <&spdifrx_endpoint>;
};
};
};
sound: sound {
compatible = "audio-graph-card";
label = "STM32MP1-DK";
routing =
"Playback" , "MCLK",
"Capture" , "MCLK",
"MICL" , "Mic Bias";
dais = <&sai2a_port &sai2b_port &sai4a_port &spdifrx_port &i2s2_port>;
status = "okay";
};
};
&i2c4 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_a>;
pinctrl-1 = <&i2c4_pins_sleep_a>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
status = "okay";
/delete-property/dmas;
/delete-property/dma-names;
cs42l51: cs42l51@4a {
compatible = "cirrus,cs42l51";
reg = <0x4a>;
#sound-dai-cells = <0>;
VL-supply = <&v3v3>;
VD-supply = <&v1v8_audio>;
VA-supply = <&v1v8_audio>;
VAHP-supply = <&v1v8_audio>;
reset-gpios = <&gpioz 7 GPIO_ACTIVE_LOW>;
clocks = <&sai2a>;
clock-names = "MCLK";
status = "okay";
cs42l51_port: port {
#address-cells = <1>;
#size-cells = <0>;
cs42l51_tx_endpoint: endpoint@0 {
reg = <0>;
remote-endpoint = <&sai2a_endpoint>;
frame-master;
bitclock-master;
};
cs42l51_rx_endpoint: endpoint@1 {
reg = <1>;
remote-endpoint = <&sai2b_endpoint>;
frame-master;
bitclock-master;
};
};
};
};
&sai2 {
clocks = <&rcc SAI2>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "x8k", "x11k";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&sai2a_pins_a>, <&sai2b_pins_b>;
pinctrl-1 = <&sai2a_sleep_pins_a>, <&sai2b_sleep_pins_b>;
status = "okay";
sai2a: audio-controller@4400b004 {
#clock-cells = <0>;
dma-names = "tx";
clocks = <&rcc SAI2_K>;
clock-names = "sai_ck";
status = "okay";
sai2a_port: port {
sai2a_endpoint: endpoint {
remote-endpoint = <&cs42l51_tx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
};
sai2b: audio-controller@4400b024 {
dma-names = "rx";
st,sync = <&sai2a 2>;
clocks = <&rcc SAI2_K>, <&sai2a>;
clock-names = "sai_ck", "MCLK";
status = "okay";
sai2b_port: port {
sai2b_endpoint: endpoint {
remote-endpoint = <&cs42l51_rx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
};
};
&sai4 {
clocks = <&rcc SAI4>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "x8k", "x11k";
status = "okay";
sai4a: audio-controller@50027004 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&sai4a_pins_a>;
pinctrl-1 = <&sai4a_sleep_pins_a>;
dma-names = "tx";
clocks = <&rcc SAI4_K>;
clock-names = "sai_ck";
st,iec60958;
status = "okay";
sai4a_port: port {
sai4a_endpoint: endpoint {
remote-endpoint = <&spdif_out_endpoint>;
};
};
};
};
&spdifrx {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spdifrx_pins_a>;
pinctrl-1 = <&spdifrx_pins_a>;
status = "okay";
spdifrx_port: port {
spdifrx_endpoint: endpoint {
remote-endpoint = <&spdif_in_endpoint>;
};
};
};With this device tree configuration, the following error occurs. Remove the node &sai4a_port in DASI, and audio can be used. How do I modify the node &sai4a_port
[ 4.441723] asoc-audio-graph-card sound: ASoC: sink widget Playback overwritten
[ 4.448991] asoc-audio-graph-card sound: ASoC: sink widget Capture overwritten
2020-09-08 7:25 AM
Hi @文�?� �? ,
Here are 2 or 3 questions to help me to understand the problem:
1) In your DT, cs42l51 is connected to i²C4 : could you please tell me on which board you are working on ?
2) When you say that "audio can be used", does it mean that adding &sai4a_port entry from dais list breaks cs42l51 codec rx and tx and/or spdif_in ? Could you please elaborate on what works and what doesn't work, and what you want to do.
BR,
Christophe
2020-09-09 7:37 PM
Hi Christophe G
1)Based on the STM32MP157-EV1 board to make a development board of our company, the CPU uses STM32MP157D, and the PMIC is removed.The audio is based on STM32MP157C-DK2
2)Yes,&Sai4a_port will destroy the RX and TX of the CS42l51 encoder
/***The audio will work normally in this way**/
dais = <&sai2a_port &sai2b_port &spdifrx_port &i2s2_port>;
dais = <&sai4a_port &spdifrx_port &i2s2_port>;
As long as CS42L51 and &sai4a_port are both in dasi, CS42L51 will report the following error
[ 4.441723] asoc-audio-graph-card sound: ASoC: sink widget Playback overwritten
[ 4.448991] asoc-audio-graph-card sound: ASoC: sink widget Capture overwritten
I think &sai4a_port and CS42L51 can run normally
2020-09-11 7:00 AM
Hi @文�?� �? ,
We had this kind of error in the past with digital microphone DT entries : the problem was coming from dapm widget names and audio interfaces which were identicals.
It has been fixed by adding a prefix :
dmic1: dmic-1 {
compatible = "dmic-codec";
#sound-dai-cells = <1>;
+ sound-name-prefix = "dmic1";
status = "okay";Hope it will help,
BR,
Christophe
2020-09-16 3:19 AM
Hi Christophe G
I am not very good at audio device tree, can you answer in detail