2023-07-20 3:33 AM
Hello,
We are using the STM32MP151 custom board microprocessor with an external flash memory (emmc). At start-up the board and linux boot correctly, but when reboot it, the board keeps in uart/usb boot loader mode and doesn't boot. It happen also when we reboot with a push button in rst pin and with software reboot.
When we reboot in software reboot, the last traces we get are:
Could you help us? Thanks.
Regards.
2023-07-20 4:55 AM
HI @Ma_mh1
Maybe you are using power discrete (no STPMIC1) and you do not connect correctly the NRST_CORE pin (see AN5031 or ES0438)
If not the root cause, dump and analyze ROM boot traces using STLINK : https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer ?
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.