cancel
Showing results for 
Search instead for 
Did you mean: 

Custom STM32MP157F Board – PANIC at PC 0x2FFEADA7 (Exception mode 0x16) During Boot from microSD

shreyaschandran
Associate III

Hello,

We have designed a custom board based on the STM32MP157F-DK2 platform.

The design uses the STM32MP157FAC MPU and includes the following peripherals:

MicroSD (SDMMC)

STPMIC1 PMIC

DDR3L memory

Ethernet

UART4 for console

 

My power sequencing, PMIC wiring, and clock architecture are identical to the DK2 reference schematics.

All voltage rails appear stable except the DDR rails, and SDMMC signals look correct during boot.

However, when I try to boot from the SD card and monitor UART4, I only receive the following messages:

PANIC at PC : 0x2ffeada7

Exception mode = 0x00000016 at : 0x2ffeada7

There is nothing else printed afterward.

 

From the Cortex-A7 exception codes, 0x16 indicates an Undefined Instruction exception, and the address 0x2FFEADA7 lies inside the SYSRAM area. This suggests the crash happens very early, likely during TF-A execution.

My problem is that the MPU never seems to wake up properly, and I cannot identify the exact origin of the failure.

I would appreciate guidance on what typically causes this panic on custom STM32MP1 boards, and which subsystems I should verify first (DDR initialization, PMIC I2C configuration, reset lines, boot chains, etc.).

 

Thank you in advance for any support.

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @shreyaschandran 

 

Your problem is likely an issue in TF-A device tree ( HSE clock ?) 

I advise you to look at FAQ: STM32MP1 How to bring up STM32MP1 

 

Hope it help 

 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.