cancel
Showing results for 
Search instead for 
Did you mean: 

spread spectrum on STM32MP1

MArdi
Associate II

Hi,

I have to use the spread spectrum on PLL4 on STM32MP1

I have set the pll4 in tfa and u-boot as follows

tfa

  

  pll4:st,pll@3 {

    cfg = < 1 49 11 10 1 3>;

csg = < 80 80 SSCG_MODE_CENTER_SPREAD >;

  };

u-boot

  pll4:st,pll@3 {

    cfg = < 1 49 11 10 1 7>;

    csg = < 16000 16000 SSCG_MODE_CENTER_SPREAD >;

    u-boot,dm-pre-reloc;

}

When I check the register (on linux) RCC_PPLL4CSGR the settings seems ok, but when I write SSCG_CTRL=1 on RCC_PLL4CR nothing happened.

Where I am wrong?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
PatrickF
ST Employee

Hello,

could you please elaborate a bit on 'nothing happened' ?

Spread spectrum is not/barely visible using an oscilloscope on an output signal. Need to have a spectrum analyzer to confirm the 'spread'.

Btw, for which purposes are you using Spread Spectrum ?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
MArdi
Associate II

Hi,

we have an anechoic chamber and we checked.

When I said "nothing happened" I mean that with the anechoic chamber I can't see the "spread spectrum".

We need the spread spectrum for the LCD (parallel interface), the clock is connected to pll4.

Thanks!

PatrickF
ST Employee

You already got answers using another channel, but for the sake of community view, I confirm the SSCG is not available for PLL3 and PLL4 (documentations will be updated to reflect this).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
MArdi
Associate II

thanks