cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding STM32mp157A UART in U BOOT

Sindhu Vadde
Associate III

Hi,

We are using stm32mp157a processor and we are working on uboot-v2018.11 at Linux side. I have an idea on board-debug-uart_init().

Path for board_debug_uart_init().

Path :board/st/stm32mp1/board.c

In board-debug-uart_init() .We have only UART_TX information i.e They configured only UART_TX pin in board_debug_uart_init() function.I need to know where will we configure UART_RX pin.

Refer the below link for uboot-v2018.11 source code Analysis.

https://elixir.bootlin.com/u-boot/v2018.11/source

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Kevin HUBER
ST Employee

Hi @Sindhu Vadde​ ,

I don't know if you still need an answer, but this function board_debug_uart_init() is used for debugging the u-boot.

So since there is only debug traces on this port, only the UART_TX is needed.

You can find information about the debug of U-Boot in this page:

https://wiki.st.com/stm32mpu/wiki/U-Boot_-_How_to_debug#Debug_with_console

Remember that you have to adapt the function board_debug_uart_init(): that configures the required resources (pad, clock) before initialization by the U-Boot driver.

This function needs to be adapted for your board.

Regards,

Kévin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
Kevin HUBER
ST Employee

Hi @Sindhu Vadde​ ,

I don't know if you still need an answer, but this function board_debug_uart_init() is used for debugging the u-boot.

So since there is only debug traces on this port, only the UART_TX is needed.

You can find information about the debug of U-Boot in this page:

https://wiki.st.com/stm32mpu/wiki/U-Boot_-_How_to_debug#Debug_with_console

Remember that you have to adapt the function board_debug_uart_init(): that configures the required resources (pad, clock) before initialization by the U-Boot driver.

This function needs to be adapted for your board.

Regards,

Kévin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here