cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with M28W320ECT 3V Supply Flash Memory hardware defect

TMlyn.1
Associate

 we are using M28W320ECT 3V Supply Flash Memory for more than 10 years wo any problems in our MCU units now, suddenly in new production this part is gone defect several times- drawing current on the 12V programming Voltage Input, no read /write operation anymore, design wasn't changed, Voltages aso also checked( Especially 12V is OK), everything correct,

Any experience or hint what else could be a root cause for this

any comment appreciated, thks&rgds, Thomas

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Alexander Czajor
Community manager

Are you sure you are using original parts form ST production?

Hi,

I think this other post has been removed because it was a duplication of this one.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
PatrickF
ST Employee

Hi @TMlyn.1​ 

For this kind of support (very old ST product and no such topic in ST Community), I recommend to create a ticket using Submit Support Request.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here