2021-12-22 2:51 AM
Hi,
I am trying to integrate swupdate for OTA update integration for STM32MP1.
In the due process I will be in need to modify the flash layout file a bit , since I am trying have an extra rootfs partition , named partition B on /dev/mmcblkp06.
I referred to flash layout currently mentioned here.
It looks to me that there is not any support for the extra rootfs which is provided.
How can i do that?
I am sure that I will be in need to change the flashlayout but since offsets are defined static in the mentioned link , I was wondering what should be offset calculation for achieving the same.
I want to achieve following scheme:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157c-ev1-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157c-ev1-trusted.bin
P 0x04 fsbl1 Binary mmc1 boot1 arm-trusted-firmware/tf-a-stm32mp157c-ev1-emmc.stm32
P 0x05 fsbl2 Binary mmc1 boot2 arm-trusted-firmware/tf-a-stm32mp157c-ev1-emmc.stm32
PD 0x06 fip Binary mmc1 0x00080000 fip/fip-stm32mp157c-ev1-trusted.bin
P 0x10 boot System mmc1 0x00480000 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs FileSystem mmc1 0x04480000 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc1 0x05480000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x13 rootfs2 FileSystem mmc1 ?????????? st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x14 userfs FileSystem mmc1 ?????????? st-image-userfs-openstlinux-weston-stm32mp1.ext4What shall be value at the place where I have mentioned ----> "??????????"
TIA
Solved! Go to Solution.
2021-12-22 5:16 AM
Hi @NPal.2 ,
You can customized the flashlayout as per your need since you respect the recommendation for partition size
STM32CubeProgrammer flashlayout - stm32mpu
Offset is just the addition of each partition size.
The flashlayout on wiki allocate 746MB to rootfs ( you can change it )
So if you want to double it, it would give something like :
P 0x12 rootfs FileSystem mmc1 0x05480000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x13 rootfs2 FileSystem mmc1 0x33E80000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x14 userfs FileSystem mmc1 0x62880000 st-image-userfs-openstlinux-weston-stm32mp1.ext4Hope it help
Olivier
2021-12-22 5:16 AM
Hi @NPal.2 ,
You can customized the flashlayout as per your need since you respect the recommendation for partition size
STM32CubeProgrammer flashlayout - stm32mpu
Offset is just the addition of each partition size.
The flashlayout on wiki allocate 746MB to rootfs ( you can change it )
So if you want to double it, it would give something like :
P 0x12 rootfs FileSystem mmc1 0x05480000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x13 rootfs2 FileSystem mmc1 0x33E80000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x14 userfs FileSystem mmc1 0x62880000 st-image-userfs-openstlinux-weston-stm32mp1.ext4Hope it help
Olivier
2021-12-22 10:46 PM
Hi @Community member : Thanks for the response. I just modified few set of things in the file :
./meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc
Added below lines :
ROOTFS2_PARTITION_SIZE ?= "${IMAGE_ROOTFS_MAXSIZE}"
PARTITIONS_CONFIG[rootfs2] ?= "${IMAGE_BASENAME},rootfs2,,${ROOTFS_PARTITION_SIZE},FileSystem"with I got the flashlayout generated according to my need.
Thanks for the inputs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.