2021-12-21 11:21 AM
IDE suggested that I upgrade STLink FW on my STM32MP1-DK2 discovery board. Now when I connect my Linux PC to USBC on DK2, device isn't recognized by STMProgrammer (also nothing shows up in dmesg).
Solved! Go to Solution.
2021-12-21 11:38 PM
Hi @BBeck.1 ,
There's no relation between ST-Link and USBC on DK2.
It's 2 different physical ports on board and drivers on PC side.
When you say IDE ? You mean STM32CubeIDE ?
>> USBC on DK2, device isn't recognized by STMProgrammer
Using CubeProg GUI ? Do you select USB as device for connection ?
Do you set boot switch to 00 for serial boot ?
Could you send a screenshot ?
>> also nothing shows up in dmesg
This case you mean with SDCard boot.
Nothing display on ST-Link Virtual Com Port console, right ?
But does the boot looks to happen with demo launcher displayed on sreen ?
Thanks
Olivier
2021-12-21 11:38 PM
Hi @BBeck.1 ,
There's no relation between ST-Link and USBC on DK2.
It's 2 different physical ports on board and drivers on PC side.
When you say IDE ? You mean STM32CubeIDE ?
>> USBC on DK2, device isn't recognized by STMProgrammer
Using CubeProg GUI ? Do you select USB as device for connection ?
Do you set boot switch to 00 for serial boot ?
Could you send a screenshot ?
>> also nothing shows up in dmesg
This case you mean with SDCard boot.
Nothing display on ST-Link Virtual Com Port console, right ?
But does the boot looks to happen with demo launcher displayed on sreen ?
Thanks
Olivier
2021-12-22 7:43 AM
Thanks. Yeah, I hadn't plugged in the OTHER usbc port (which is the DFU) on the DK2 board. Anyhow, it was coincidental that The Cube IDE prompted for ST-link upgrade.
I appreciate your response.
Cheers,
Ben
2021-12-22 7:46 AM
Hi @BBeck.1
Thanks for feedback !
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.