cancel
Showing results for 
Search instead for 
Did you mean: 

I have a board from arrow called avenger96 that uses a STM32MP157ACCx, it is making a odd buzzing sound when i power it up which i can not explain.

TGhau.2088
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
PatrickF
ST Employee

Hello, please check this issue with Arrow. Usually linked to SMPS inductors. Noise could disappear when power load increase.

Not linked to STM32MP15 component.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

I don't have the board, but in general some switching supplies will whistle / squeal at the edge of the hearing range, the pitch / presence can change with loading, or lack of it.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Martin Devera
Associate III

Also it is very often MLCC capacitor. There is simple test, take srewdriver and touch (don't short!) ceramit part of capacitors and inductors. When spotting correct one, the sound will change. MLCCs with class 2 dielectrics are quite a lot microphonics.