2022-08-09 1:41 AM
I`ve built st-image-weston for stm32mp157f-disco board with flutter and clang layer. Then I built SDK with:
bitbake core-image-weston -c populate_sdkThen I installed SDK with
.tmp/deploy/sdk/core-image-weston-openstlinux-weston-stm32mp15-disco-x86_64-toolchain-4.0.1-snapshot.shAfter that I setup environment with
source /opt/st/stm32mp15-disco/4.0.1-snapshot/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
export CC=${CLANGCC}
export CXX=${CLANGCXX}My question is how can I install a simple flutter app to my discovery board. What are the steps that I need to follow.
Solved! Go to Solution.
2022-08-25 7:59 AM
@Gencay This is not a simple answer.
First it depends on what image type you have (runtime=debug, runtime=release, runtime=profile).
My experience is that running a Flutter app via debug on the STM32MP157F-DK2 is very slow. So I would avoid that for now.
If you have a runtime=release image, then you have to create an AOT image.
The steps used by meta-flutter to generate an AOT (release - libapp.so) is located here:
https://github.com/meta-flutter/meta-flutter/blob/kirkstone/classes/flutter-app.bbclass#L170
If you install the flutter-engine-<runtime flavor>-sdk-dev package to image, you can scp the engine_sdk.zip from /usr/share/flutter/engine_sdk.zip. This has required gen_snapshot to generate an AOT image.
So once you have the libapp.so you create your bundle folder on target. This can be in /tmp or wherever you have write access to.
Create this folder structure on target. data/flutter_assets is from your host build/flutter_assets folder.
<bundle folder>
data
flutter_assets
lib
libapp.so
For DRM run:
`flutter-pi --release <bundle folder>`
For Wayland run:
`flutter-auto --w=1920 --h=720 --b=<bundle folder>
I may have missed something but that's the general flow. Feel free to start a discussion here so other meta-flutter users can benefit:
https://github.com/meta-flutter/meta-flutter/discussions
Cheers,
Joel
2022-08-25 7:21 AM
Hi @Gencay ,
@Community member (Kudos to him ! ) share his Flutter project for MP1 here in this community :
https://community.st.com/s/project/a8g3W000000fxV5QAI/google-flutter-for-stm32mp1
I'm quite sure this will help you
Olivier
2022-08-25 7:59 AM
@Gencay This is not a simple answer.
First it depends on what image type you have (runtime=debug, runtime=release, runtime=profile).
My experience is that running a Flutter app via debug on the STM32MP157F-DK2 is very slow. So I would avoid that for now.
If you have a runtime=release image, then you have to create an AOT image.
The steps used by meta-flutter to generate an AOT (release - libapp.so) is located here:
https://github.com/meta-flutter/meta-flutter/blob/kirkstone/classes/flutter-app.bbclass#L170
If you install the flutter-engine-<runtime flavor>-sdk-dev package to image, you can scp the engine_sdk.zip from /usr/share/flutter/engine_sdk.zip. This has required gen_snapshot to generate an AOT image.
So once you have the libapp.so you create your bundle folder on target. This can be in /tmp or wherever you have write access to.
Create this folder structure on target. data/flutter_assets is from your host build/flutter_assets folder.
<bundle folder>
data
flutter_assets
lib
libapp.so
For DRM run:
`flutter-pi --release <bundle folder>`
For Wayland run:
`flutter-auto --w=1920 --h=720 --b=<bundle folder>
I may have missed something but that's the general flow. Feel free to start a discussion here so other meta-flutter users can benefit:
https://github.com/meta-flutter/meta-flutter/discussions
Cheers,
Joel
2022-09-12 3:54 AM
I have unzip this file
/usr/share/flutter/engine_sdk.zip, then I have
engine_sdk/sdk/clang_x64/gen_snapshot directory at the target. After this how can I generate my AOT image?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.