2022-06-06 3:20 AM
Hello ,
Currently, i am working on STM32MP157.
I am trying to change the device tree USB type C configuration into a USB type A host.
I've disabled usbotg option under stm32mp1571.dtsi file. I would like to know where i could add USB A host configuration.
Thank you
Solved! Go to Solution.
2022-06-08 8:29 AM
Hello Kevin,
Thank you for contacting me.
I made some mistakes in the compilation. After proper compilation, I could use both USB (usbphyc_port1,usbphyc_port0 ) as USBH.
Regards
SJ
2022-06-06 5:59 AM
HI @JSIGA.1
Do you want to add an USB Type-A config on OTG (USB_DP2/USB_DM2 pins) or just force the OTP in host mode (with USB micro-A)?
Note that OTG is not intended to be a full Type-A as it does not support USB Hub and has probably lower performances than USBH.
For host usages, it is recommended to use USBH which could manage two external ports on port0 and port1 (respectively USB_DP1/USB_DM1 and USB_DP2/USB_DM2 pins)
See https://wiki.st.com/stm32mpu/wiki/USBH_device_tree_configuration.
Regards.
2022-06-06 8:52 AM
Hello,
Thank you for your response.
My case is USB_DP1/USB_DM1 is configured as USBH and USB_DP2/USB_DM2 is configured as Type-C.
I am trying USB_DP2/USB_DM2 to configure as USBH.
I've tried disabling "usbotg_hs" disabled and added 2 physical port in USBH configuration.
&usbh_ehci {
phys = <&usbphyc_port0>, <&usbphyc_port1 1>;
phy-names = "usb","usb";
status = "okay";
};
&usbh_ohci {
phys = <&usbphyc_port0>, <&usbphyc_port1 1>;
phy-names = "usb","usb";
status = "okay";
};
&usbphyc {
status = "okay";
};
&usbotg_hs{
status = "disabled";
};
USBH (USB_DP2/USB_DM2) not detect any USB devices .
2022-06-06 11:45 PM
Hi,
not expert, but maybe missing some entries in &usbphyc node (e.g. 'connector' )
https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration#DT_configuration_example
Maybe share more details on your issue (e.g.. log files)
Regards,
Patrick
2022-06-08 2:35 AM
Hello @JSIGA.1 ,
Your configuration seems consistent with what you are trying to do.
As wrote by Patrick, we will need several information to help you.
Please can you send us:
Regards,
Kevin
2022-06-08 8:29 AM
Hello Kevin,
Thank you for contacting me.
I made some mistakes in the compilation. After proper compilation, I could use both USB (usbphyc_port1,usbphyc_port0 ) as USBH.
Regards
SJ
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.